Technical FAQs

Ask a Question

Will any other current protection be turned off as well if the motor overload protection is turned off on the Altivar ATV66?

No just the thermal. The overcurrent will still be active. And all other faults as well.

CTA-ID : 7099
Was this helpful?
What can we do to improve the information ?