Technical FAQs

Ask a Question

What does NLP indicate on the Altivar ATV66?

It stands for No Line Power present on unit`s L1, L2 and L3 power terminals, drive would be separately supplied with control power to the CL1 and CL2 control terminals.

CTA-ID : 7091
Was this helpful?
What can we do to improve the information ?