Technical FAQs

Ask a Question

Is the type N Altivar ATV58 UL listed?

Yes.
UL Listed per UL 508C as incorporating electronic overload protection.
UL File E138755 CCN NMMS
cUL Listed per Canadian Standard C22.2 No. 14.
CSA File LR60905
Conforms to applicable NEMA ICS, NFPA, IEC, and ISO 9001 standards.


CTA-ID : 6803
Was this helpful?
What can we do to improve the information ?