Technical FAQs

Ask a Question

What is the required torque for the CU250KA lug for the KA and KH breakers?

250 lb-in (29 N-M)


CTA-ID : 6436
Was this helpful?
What can we do to improve the information ?