Technical FAQs

Ask a Question

Which wire sizes are approved for the AL250KIT lug for the KI and KC breakers?

1/0 AWG-350 kcmil (50-185 mm2)


CTA-ID : 6413
Was this helpful?
What can we do to improve the information ?