Technical FAQs

Ask a Question

Which wire sizes are approved for the AL250KI lug for the KI and KC breakers?

1/0 AWG-350 kcmil (50-185 mm2)


CTA-ID : 6412
Was this helpful?
What can we do to improve the information ?