Technical FAQs

Ask a Question

What is required to get the ATS46 to communicate via Modbus protocol?

To communicate via Modbus RTU, Modbus ASCII, UNI-TELWAY, and ASCII Protocol for PC with the ATS46 unit the module part number VW3G46301U is required.  

With this module present on unit you can communicate via hyperterminal which is available on Windows software.

Also, need a cable to connect the PLC communication module to the PC`s serial COM port you will need a cable which can get from Square D using part number VY1G461510.

CTA-ID : 7403
Was this helpful?
What can we do to improve the information ?