Technical FAQs

Ask a Question

What is the speed regulation of the Altivar ATV66 drives?

Volts/Hertz control type:
determined by motor slip, 3% typical for Nema B motor
Normal or High Torque (sensorless flux vector) control type:
1.0% without adjustments
0.5% with optional Tachometer


CTA-ID : 7081
Was this helpful?
What can we do to improve the information ?