Technical FAQs

Ask a Question

Why are the input line current ratings for the ATV66 different depending on the Available interrupting current (AIC)?

The higher AIC systems have lower system impedance therefore it has more current distortion which leads to a higher input current rating.

CTA-ID : 7076
Was this helpful?
What can we do to improve the information ?