Technical FAQs

Ask a Question

Can the electrician wire the ground to a screw at the base of the Altivar ATV56 because they did not pull a ground wire to the drive when they pulled the power?

No, the ground must be at the same potential as the system ground.

CTA-ID : 6776
Was this helpful?
What can we do to improve the information ?