Technical FAQs

Ask a Question

Can the Altivar ATV66 internal 24VDC supply power an external transducer.

It can be used providing the total logic input power and transducer power required does not exceed 210mA. If an external short occurs on the transducer it could possibily damage the drives internal supply.


CTA-ID : 6774
Was this helpful?
What can we do to improve the information ?