Technical FAQs

Ask a Question

Which wire sizes will the CVC250KA3 lug for the circuit breakers KA, KH, KC, KI accept?

2/0 AWG-300 kcmil (70-150 mm2) copper only


CTA-ID : 6410
Was this helpful?
What can we do to improve the information ?