Technical FAQs

Ask a Question

Can the Altistart ATS46 talk Devicenet?

The only communications protocols that are used are Modbus, Uni-Telway & JBUS. This requires part number VW3G46301U. It may be possible to get a third party bridge to convert Modbus to device net.

CTA-ID : 7391
Was this helpful?
What can we do to improve the information ?