Technical FAQs

Ask a Question

Will the Altistart ATS46 work on 208 volts?

Issue: Will the Altistart ATS46 work on 208 volts?
 
Product Line: ATS46
 
Environment: All
 
Cause: N/A
 
Resolution: Yes that is in range for the the ATS46 family of softstarts.


 
Was this helpful?
What can we do to improve the information ?