Technical FAQs

Ask a Question

What is the sampling rate of the Logic Inputs on the Altivar ATV66 drive?

The sampling rate of Logic Inputs is 10 ms.


CTA-ID : 7072
Was this helpful?
What can we do to improve the information ?