Technical FAQs

Ask a Question

What is specifications on Q207 mod for the 8839 enclosed Altivar ATV66 regarding the coil rating on the relay?

The coil rating is 115V on the relay. Talked to Teresa and she said if customer has bypass then the relay rating should be 115V and 24V for one without bypass.


CTA-ID : 7067
Was this helpful?
What can we do to improve the information ?