Technical FAQs

Ask a Question

How does the drive determine the number of motor poles to be able to display speed in RPM on the Altivar ATV66?

Need to enter the motor rated RPM in menu 4 when selecting to display motor speed.


CTA-ID : 7064
Was this helpful?
What can we do to improve the information ?