Technical FAQs

Ask a Question

What is the part number for a signal isolation module that can be used on the 4-20mA speed reference coming from a PLC and inputting into the Altivar ATV66?

The part number is 52011-889-50.

CTA-ID : 7057
Was this helpful?
What can we do to improve the information ?