Technical FAQs

Ask a Question

Does the Altivar ATV66 have automatic restart?

Yes the automatic restart feature allows up to 5 restart attempts after the unit has tripped on a fault and set this up in menu 7.4. The time between restart attempts is adjustable from 1-600 seconds.

CTA-ID : 7051
Was this helpful?
What can we do to improve the information ?