Technical FAQs

Ask a Question

Does the ATV56 it meet CE complience?

No the ATV56 does not have a declaration of conformity statement because it is for use only in the US. Would have to use an ATV66 outside of the US.

CTA-ID : 6770
Was this helpful?
What can we do to improve the information ?