Technical FAQs

Ask a Question

What is the polution degree for the Altivar ATV56 unit?

Told him it was Polution degree 3 per NEMA ICS-1 and IEC 664-1


CTA-ID : 6767
Was this helpful?
What can we do to improve the information ?