Technical FAQs

Ask a Question

How does input phase inbalance operate on the Altivar ATV56?

Told him that if there is a phase imbalance of 18 to 20% then would get input phase fault. If it voltage drops low in one phase (below the -15% ) Would get under supply fault.

CTA-ID : 6761
Was this helpful?
What can we do to improve the information ?