Technical FAQs

Ask a Question

Will the PCMCIA card allow me to load preset configurations on the Altivar ATV56?

This card allows for the storage of up to 16 files that he must create in the drive.


CTA-ID : 6754
Was this helpful?
What can we do to improve the information ?