Technical FAQs

Ask a Question

What are the differences between the ATS23 pump controller and the standard version?

The pump controller had two selectable deceleration ranges (1-60 seconds and 2-120 seconds), a selectable prealarm circuit / load ouptut relay (either overload or underload, for loss of suction, annunciation), an adjustable voltage range for decel, and automatic deceleration ramp adaption based on load requirements. The ramp adaptation also had a potentiomter associated with it that set the rated motor feedback.

In contrast, the standard versionl had two selectable stopping modes (decelerated or DC injection braking), a selectable starting boost function (5 cycles of full voltage before applying ramp time), and did not monitor actual motor voltage during deceleration.

CTA-ID : 6365
Was this helpful?
What can we do to improve the information ?