Technical FAQs

Ask a Question

Will the GFM will work on a single phase circuit?

Yes. If the circuit uses one pole and neutral, the included neutral current transformer must be used.


CTA-ID : 6357
Was this helpful?
What can we do to improve the information ?