Technical FAQs

Ask a Question

What is the part number for the blue plate on the top of the 8803 omegapak unit which houses the line terminals?

This is not a part that can be ordered.  In order to get it replaced, return the drive to the depot for repair.

CTA-ID : 4020
Was this helpful?
What can we do to improve the information ?