Technical FAQs

Ask a Question

Which DC voltages are available for the NSJ motor operators?

The motor operator for the NSJ is available in the following DC voltages:
Voltage Suffix
24/30 MO
48/60 MP
110/130 MR
250 MS



CTA-ID : 6341
Was this helpful?
What can we do to improve the information ?