Technical FAQs

Ask a Question

Can you get an Altistart ATS46 softstart with full voltage bypass?

Issue: Can you get an Altistart ATS46 softstart with full voltage bypass?
 
Product Line: ATS46 8638 8639
 
Environment: Enclosed ATS46
 
Cause: N/A
 
Resolution: It is available with some enclosed units as an option.

With 8638 (Fusible disconnect) units or 8639 (Circuit breaker disconnect) enclosed soft starters the full voltage bypass is option Z24

This option is NOT available with 8636 (non-combination) type enclosed units.

 
Was this helpful?
What can we do to improve the information ?