Technical FAQs

Ask a Question

Will the Altistart ATS46 or ATS48 complete deceleration before it will accept another start signal?

Whenever a stop command is given, even if only momentary, the soft starter will complete the stop cycle before restarting.
If a start command is given before the stop cycle is complete, the soft starter will begin to start as soon as the stop cycle is done unless the time before restart (TbS) feature is being used. If TbS is set, then the soft starter will wait for the set time period before restarting.

CTA-ID : 7361
Was this helpful?
What can we do to improve the information ?