Technical FAQs

Ask a Question

What is modification Q404 on the 8839 enclosed Altivar ATV66?

Q404 is a secondary surge arrestor which provides supplementary MOV protection using a class 6671 SDSA3650 Surgebreaker secondary surge arrestor hard wired and factory mounted.


CTA-ID : 7049
Was this helpful?
What can we do to improve the information ?