Technical FAQs

Ask a Question

Does the Altivar 58 Type N come with a keypad?

Type N drive can be ordered with or without the keypad included.
Complete the catalog number with KU for ATV58 TRX Type N controllers with factory-installed keypad,
or ZU for controllers without a factory-installed keypad. For catalog numbers ending in ZU, an operator interface
must be used to modify factory settings. Order separately. Refer to Appendix A or catalog 8806CT9901 for
available interface options.

CTA-ID : 6747
Was this helpful?
What can we do to improve the information ?