Technical FAQs

Ask a Question

Why is Altivar ATV56 getting a random stop command while running?

Possibly due to noisy power supply causing an eroneous stop command on the keypad, especially if have a jumper from +24 to Li1 and LI2. The part number for the keypad is VW3A66206U.


CTA-ID : 6733
Was this helpful?
What can we do to improve the information ?