Technical FAQs

Ask a Question

Which AC voltages are available for the NSF motor operators?

The motor operator for the NSF is available in the following AC voltages:
Volts Suffix
48/60 ML
110/130 MA
208/277 MD
380/480 MH

CTA-ID : 6331
Was this helpful?
What can we do to improve the information ?