Technical FAQs

Ask a Question

Can you have 3 pilot lights on his 8639 Altistart ATS46 softstart?

Issue: Can you have 3 pilot lights on his 8639 Altistart ATS46 softstart?
 
Product Line:  Enclosed ATS46
 
Environment: All
 
Cause: N/A
 
Resolution: Yes, the control island will hold up to 6 operators.


 
Was this helpful?
What can we do to improve the information ?