Technical FAQs

Ask a Question

Will the Altstart ATS46 operate at 50 Hz and 380 volts?

Issue: Will the Altstart ATS46 operate at 50 Hz and 380 volts?
 
Product Line: ATS46
 
Environment: All
 
Cause: N/A
 
Resolution: Yes it will.


 
Was this helpful?
What can we do to improve the information ?