Technical FAQs

Ask a Question

What are the bus bars made of for a high HP Altistart ATS46 softstart?

Issue: What are the bus bars made of for a high HP Altistart ATS46 softstart?
 
Product Line: ATS46
 
Environment: All
 
Cause: N/A
 
Resolution: Tin plated copper.


 
Was this helpful?
What can we do to improve the information ?