Technical FAQs

Ask a Question

Where are the bus connections for the ATS46 soft starters.

Issue: Where are the bus connections for the ATS46 soft starters.
 
Product Line: ATS46 Softstarters
 
Environment: All
 
Cause: N/A
 
Resolution: Any bus connections are on the bottom. Connections that are on the top are not the bus type. Also, only the ATS46C17N and larger use bus connections.


 
Was this helpful?
What can we do to improve the information ?