Technical FAQs

Ask a Question

Is an Altistart ATS46 thyristor and a SCR module the same?

Issue: Is an Altistart ATS46 thyristor and a SCR module the same?
 
Product Line: ATS46
 
Environment: All
 
Cause: N/A
 
Resolution: The words are interchangeable.


 
Was this helpful?
What can we do to improve the information ?