Technical FAQs

Ask a Question

Can an Altivar ATV66 drive cause even harmonics?

Providing the input line current on all phases is balanced the drive will not cause even harmonics. If input current is not balanced check for balanced voltage or an open or non-conducting diode on one phase.

CTA-ID : 7014
Was this helpful?
What can we do to improve the information ?