Technical FAQs

Ask a Question

Can you hook a 0 - 10v signal up on AI2 of the Altivar ATV56?

No, AI2 is used with a 4-20 ma or 0-5V signal. If already using a speed pot as well, will have to get an I/O extension module and use AI3 for 0-10V input.

CTA-ID : 6730
Was this helpful?
What can we do to improve the information ?