Technical FAQs

Ask a Question

Why do we require fuses on the line of Altivar ATV56?

The drive does not have a AIC rating without a fuse which is how it was tested. The manual requires a fuse to protect the front; without a fuse the drive may not be covered under warranty if a bolted fault occurs and the drive is damaged.


CTA-ID : 6727
Was this helpful?
What can we do to improve the information ?