Technical FAQs

Ask a Question

How is over speed fault on the Altivar ATV66 disabled?

Set the ``control spd + err`` parameter in Menu 7.4 to ``No``. This Fault occurs when the motor is running at a speed higher than being commanded to run by the speed reference.

CTA-ID : 6723
Was this helpful?
What can we do to improve the information ?