Technical FAQs

Ask a Question

How can you get rid of over speed fault on the Altivar ATV56 because it is a nuisance?.

Can simply disable the ``control spd + err`` in Menu 7.4 if this is a nuisance. Fault occurs when the output is running at a frequency higher than being commanded to run by the speed reference.


CTA-ID : 6722
Was this helpful?
What can we do to improve the information ?