Technical FAQs

Ask a Question

Is the motor overload protection disabled when Output Phase loss is disabled on Altivar ATV56 8839 Bele Box?

The motor overload protection is not disabled by disabling the output phase fault. Output phase fault protection is a single phase protection. If a single phase does go out, the higher currents in other phases get picked up and the drive trips.

CTA-ID : 6718
Was this helpful?
What can we do to improve the information ?