Technical FAQs

Ask a Question

Are the SCRs the same part number for Altistart ATS46 as for Altistart ATS23?

Issue:   Are the SCRs the same part number for Altistart ATS46 as for Altistart ATS23?
 
Product Line:   ATS23 ATS46
 
Environment:  All
 
Cause:   N/A
 
Resolution:   Yes, they are the same part numbers for the corresponding sizes.


 
Was this helpful?
What can we do to improve the information ?