Technical FAQs

Ask a Question

What size strip heater should you use in an 8639 Altistart ATS46, 60HP unit?

Issue: Sizing strip heater
 
Product Line:  Enclosed ATS46
 
Environment: All
 
Cause: N/A
 
Resolution: Need to contact the strip heater manufacturer and the size of the enclosure will determine which strip heater is needed.


 
Was this helpful?
What can we do to improve the information ?