Technical FAQs

Ask a Question

How can we provide a customer with a 0-5vdc signal proportional to load current on an Altistart ATS46?

Can use an isolation / converter device but there are two problems: 1) added cost of converter; 2) the convert would require a power supply.


CTA-ID : 7313
Was this helpful?
What can we do to improve the information ?