Technical FAQs

Ask a Question

How is Motor Power Calculated on the Altivar ATV66?

The drive monitors the voltage and current which is used to calculate power.


CTA-ID : 7010
Was this helpful?
What can we do to improve the information ?