Technical FAQs

Ask a Question

Can the Altivar ATV66 DC inject the motor on a start command without adding external wiring and control.

No, would need to add wiring to a logic input to act as a DC injection stop. Programming would be done in menu 7.2 under Controlled Stop.

CTA-ID : 7008
Was this helpful?
What can we do to improve the information ?