Technical FAQs

Ask a Question

What is the speed regulation of the Altivar ATV66 unit?

Volts/hertz control type (VT or VTLN) is typically 3%. Normal or high troque control type (CT) is 1.0% without adjustments or 0.05% with optional I/O extension card and tachometer input


CTA-ID : 7006
Was this helpful?
What can we do to improve the information ?